9DoF Sensor Stick Hookup Guide

Pages
Contributors: Alex the Giant
Favorited Favorite 0

Introduction

The 9DoF Sensor Stick is an easy-to-use 9 degrees of freedom IMU. The sensor used is the LSM9DS1, the same sensor used in the SparkFun 9 Degrees of Freedom IMU Breakout, but is slimmed down to be only 0.9"x0.4".

SparkFun 9DoF Sensor Stick

SEN-13944
8 Retired

Required Materials

To follow along with this hookup guide, you will need the following:

Suggested Reading

Before getting started, you may find the following links useful:

Pull-up Resistors

A quick introduction to pull-up resistors - whey they're important, and how/when to use them.

Installing an Arduino Library

How do I install a custom Arduino library? It's easy! This tutorial will go over how to install an Arduino library using the Arduino Library Manager. For libraries not linked with the Arduino IDE, we will also go over manually installing an Arduino library.

Gyroscope

Gyroscopes measure the speed of rotation around an axis and are an essential part in determines ones orientation in space.

How to Use a Breadboard

Welcome to the wonderful world of breadboards. Here we will learn what a breadboard is and how to use one to build your very first circuit.

Logic Levels

Learn the difference between 3.3V and 5V devices and logic levels.

Accelerometer Basics

A quick introduction to accelerometers, how they work, and why they're used.

I2C

An introduction to I2C, one of the main embedded communications protocols in use today.

Hardware Overview

Let's go over the 9DoF Sensor Stick in detail.

9DoF Sensor Stick

LSM9DS1 Details:

  • 3 acceleration channels, 3 angular rate channels, 3 magnetic field channels
  • ±2/±4/±8/±16 g linear acceleration full scale
  • ±4/±8/±12/±16 gauss magnetic full scale
  • ±245/±500/±2000 dps angular rate full scale
  • I2C serial interface
  • Operating Voltage: 3.3V

Pull-up Resistors

This breakout board has built-in 4.7 kΩ pull up resistors for I2C communications. If you're hooking up multiple I2C devices on the same bus, you may want to disable/enable the pull-up resistors for one or more boards. On the 9DoF Sensor Stick, the pull-ups are enabled by default. To disable them, simply use a hobby knife to cut the traces connecting the left and right pads of the jumper labeled I2C PU on the back of the board. This will disconnect the resistors on the I2C bus from VCC.

i2c pullup jumper

Changing I2C Addresses

If you're using multiple Sensor Sticks, or have a device that's already using the default addresses of the Sensor Stick, you'll want to change addresses to avoid having multiple devices try to talk over one another. The default address for the magnetometer is 0x1E and the default address for the accelerometer and gyroscope is 0x6B. To change the addresses, you'll want to use a hobby knife to cut the trace between center and top pads and use solder to short the center and bottom pads. This will change the address of the magnetometer to 0x1C and the accelerometer and gyroscope to 0x6A.

address jumper

Hardware Connections

Connecting the 9DoF Sensor Stick to an Arduino

Wiring the Sensor Stick is very easy! We recommend soldering four male headers to the sensor stick. You can also directly solder wires to the board to fit your application's needs.

Power

This board runs on 1.9V to 3.6V. Be sure to power the board from the 3.3V pin! I2C uses an open drain signaling, so there is no need to use level shifting; the 3.3V signal will work to communicate with the Arduino and will not exceed the maximum voltage rating of the pins on the LSM9DS1.

Connections to the Arduino

The 9DoF Sensor Stick has only four pins. We'll be connecting VCC and GND to the normal power pins, and the remaining two pins are used for I2C communication. If you're using a newer board that has SDA and SCL broken out, you can connect the SDA and SCL pins from the Sensor Stick directly to those pins. If you're using an older board, SDA and SCL are pins A4 and A5 respectively.

  • VCC → 3.3V
  • GND → GND
  • SDA → SDA/A4
  • SCL → SCL/A5

Your circuit should look something like this:

alt text

Installing the Arduino Library

We've written a full-featured Arduino library to help make interfacing with the LSM9DS1's gyro, accelerometer, and magnetometer as easy-as-possible. Visit the GitHub repository to download the most recent version of the library, or click the link below:

For help installing the library, check out our How To Install An Arduino Library tutorial. You need to move the SparkFun_LSM9DS1_Arduino_Library folder into a libraries folder within your Arduino sketchbook or use the Library Manger to install.

The LSM9DS1_Basic_I2C Example

To verify that your hookup works, load up the LSM9DS1_Basic_I2C example by going to File > Examples > LSM9DS1 Breakout > LSM9DS1_Basic_I2C.

The default values set by this sketch should work for a fresh, out-of-the-box 9DoF Sensor Stick -- it assumes both of the address jumpers haven't been modified. Upload the sketch, then open up your serial monitor, setting the baud rate to 115200. You should see something like this:

Example serial monitor output

The current reading from each axis on each sensor is printed out, then those values are used to estimate the sensor's orientation. Pitch is the angle rotated around the y-axis, roll is the board's rotation around the x-axis, and heading (i.e. yaw) is the sensor's rotation around the z-axis. Try rotating the board (without pulling out any wires!) to see how the values change.

Resources and Going Further

For more information about the 9DoF Sensor Stick, check out the links below:

Now that you've got the Sensor Stick up-and-running, what project are you going to incorporate motion-sensing into? Need a little inspiration? Check out some of these tutorials!

  • Dungeons and Dragons Dice Gauntlet -- This project uses an accelerometer to sense a "rolling the dice" motion. You could swap in the LSM9DS1 to add more functionality -- like compass-based damage multipliers!
  • Are You Okay? Widget -- Use an Electric Imp and accelerometer to create an "Are You OK" widget. A cozy piece of technology your friend or loved one can nudge to let you know they're OK from half-a-world away.
  • Leap Motion Teardown -- An IMU sensor is cool, but image-based motion sensing is the future. Check out this teardown of the miniature-Kinect-like Leap Motion!

Das Blinken Top Hat

A top hat decked out with LED strips makes for a heck of a wedding gift.

Qwiic Scale Hookup Guide

Create your own digital scale quickly and easily using the Qwiic Scale!

SparkFun PIR Breakout Hookup Guide

Get started with these Panasonic EKM-Series PIR breakouts following this Hookup Guide.

Qwiic Pressure Sensor (BMP581) Hookup Guide

Get started with the SparkFun Pressure Sensor - BMP581 (Qwiic) following this Hookup Guide